Issue:
What options do you have when Mounting Altivar 320 Faceplate?
Product Line:
ATV32, ATV320
Environment:
All ATV32 series, ATV320 "B" type only.
Cause:
Application requires horizontal mounting for control access.
Resolution:
The faceplate of the Bookshelf Version of the ATV320 can be mounted Horizontally. This only applies to the drives with part number ATV320..B. It will require a modification of the drive, and an additional mounting bracket will be needed. The part number for this bracket is VW3A9920.
What options do you have when Mounting Altivar 320 Faceplate?
Product Line:
ATV32, ATV320
Environment:
All ATV32 series, ATV320 "B" type only.
Cause:
Application requires horizontal mounting for control access.
Resolution:
The faceplate of the Bookshelf Version of the ATV320 can be mounted Horizontally. This only applies to the drives with part number ATV320..B. It will require a modification of the drive, and an additional mounting bracket will be needed. The part number for this bracket is VW3A9920.
Released for:Schneider Electric Global