Issue
When trying to generate a report there is an error in the browser. In the EventException table in the ION_SystemLog the following error can be seen:
An error has occurred during report processing. ---> System.Globalization.CultureNotFoundException: Culture is not supported. Parameter name: culture 4096 (0x1000) is an invalid culture identifier.
Product Line
Power Monitoring Expert 8.x
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Environment
The Region selected in Settings has been set to a custom culture, such as francais (Tunisie) or English (Sweden).
Cause
There is a known issue with the Microsoft Report Viewer control and custom cultures. See this link for more information:
Resolution
Change the Region to something different to workaround this problem.
Released for:Schneider Electric Global