{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Why am I unable to connect SoMove software to a Process Drive while it is displaying StO?

Issue:
Process Drive State is StO and is unable to connect to SoMove Software.

Product Line:
Altivar Process Drive

Environment:
ALL

Cause:
Wiring / Programming

Resolution:
StO is Safe Torque Off, which means you are unable to operate the drive with any type of Controls.  SoMove allows for operation, so therefore, SoMove can not be connected in this state.  If you've only removed the factory jumper on P24, STOA, STOB, and are not currently using a wired safety contact, simply re-install the jumper.  Remember to use 24v terminal, rather than P24, for your control wiring.

Schneider Electric Global

Explore more
Range:
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Category: