What do I do when I see Error 1392 "When using logged variable values, assign the variable to a data logging group." in the Vijeo Designer Feedback Zone?
Issue
Error 1392 "When using logged variable values, assign the variable to a data logging group." appears when a Vijeo Designer HMI project is built.
Product Line
Vijeo Designer v4.5+
Environment
Windows 7, Windows 10
Cause
When Error 1392 "When using logged variable values, assign the variable to a data logging group." appears, it means that a Variable designated for logging that was mandatory is no longer assigned . In working with data logging, you must assign the variable to a data logging group, which contains a set of properties that specifies the data collection method and data storage details for a variable.
Resolution
Assign the variable to a data logging group using the Data Details tab in the Variable Properties dialog box or in the Variable node's Logging Group column.
Released for:Schneider Electric Global
Explore more
Range:
Vijeo Designer
ELF3200 Series
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.