What amount of current imbalance is needed for EPHO fault to be triggered on the ATV212 series drives?
Published date:
22 October 2018
Issue:
EPHO fault detected, what causes this?
Product Line:
ATV212 series drives. Open style and Enclosed versions.
Environment:
All models, All serial numbers.
Cause:
Information unavailable in current literature.
Resolution:
When the current draw on any phase drops to 25% or less of the load current and remains 25% or below for 90 degrees of rotation within the phase, EPHO fault is triggered. This fault detection is designed to detect a load imbalance or an open phase(s) on the output of the drive and stop the drive.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.