How to automatically backup a PowerSCADA Expert system
Published date:
07 November 2018
Issue
Automatic backups are required for PowerSCADA Expert
Product Line
PowerSCADA Expert 8.2
Environment
Windows Task Scheduler
Cause
Automatic backups are not natively implemented within PowerSCADA Expert.
Resolution
This attached document includes the tasks required to create automated backups of a PSE system.
You can automate the backing up of PowerSCADA Expert (PSE) to include most of the PSE components that will be required to restore a system. PSE passwords and device profiles cannot be automatically backed up. They must be backed up manually. You can find the required procedure for this process starting on page 9.
Note: Some procedures in this document cite scripts you can use to automate the backup and restore process. These scripts are included in the Appendix.