Issue:
What is the NFPA Hazard Rating for Smart-UPS?
Product Line:
Smart-UPS
Environment:
All models, All Serial Numbers
Cause:
"NFPA 704: Standard System for the Identification of the Hazards of Materials for Emergency Response" is a standard maintained by the U.S.-based National Fire Protection Association. Some local jurisdictions require this information for all installed equipment
Resolution:
The NFPA Hazard Rating for non-spillable lead acid batteries is based on Sulfuric acid:
Flammability (Red) = 0
Health (Blue) = 3
Reactivity (Yellow) = 2 (Sulfuric acid is water-reactive if concentrated)
Released for:Schneider Electric Global