{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to build a part number for SagFighter™ Active Voltage Conditioner
Issue
Customer needs to build a part number for SagFighter Active Voltage Conditioner unit

Product Line
SagFighter™ Active Voltage Conditioner

Resolution
SagFighter™ Active Voltage Conditioner selection guide is attached below.

Image 1

Common ordering options can be found below. Please note standard voltages for 60 Hz systems are 208, 240, 480, 600 and for 50 Hz systems are 220, 380, 400, 415. Non-standard voltages are available.
Image 2

For further information, refer to the attached pdf.

Schneider Electric Global

Attachment(s)
SAG_Fighter_Specification_0209A.pdf [96.27 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: