{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How can I find the MAC address of a PM8000 or ION7400 meter from the front panel?
Issue
How can I find the MAC address of a PM8000 or ION7400 meter from the front panel?

Product Line
PM8000 or ION7400 meters

Environment
Metering & Power Monitoring

Cause
The customer could not find the MAC address of the PM8000 or ION7400 meter.

Resolution
Media Access Control Address (MAC address or MAC ID) is a unique identifier assigned to all network interfaces.

From the meter front panel:
  • Press on the button with the "HOME" icon
  • Use "Up" or "Down" soft key to scroll until the "Communication Setup" is highlighted on the screen
  • Press the soft key under the "Check mark" on the far right
  • Press the soft key corresponding to the "Arrow down"
  • Read the "MAC Address" that appears on the screen.