Cause: The artwork is correct. The SBP3000 is intended to be wall mounted or used in tower format.
Resolution: The SBP3000 can be rack mounted but it will have the artwork text upside down, unless the bypass panel is oriented with the AC input on the right and switch on the left.