{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
AltivarProcess variable speed drive used in installations with SCCR biger than max value of 50kA declared for ATV630...N4?
Whenever network prospective current at the point of Altivar installation is greater than the value of max prospective current defined in Altivar catalog for dedicated drive, it is mandatory to add line choke.
ATV630..N4 drives have max Isc of 50kA, so for you network with SCCR 80 or 100kA you have to use line choke. With line choke you can be sure that max Isc at Altivar inputs will always be below 50kA, despite whatever high SCCR upstream the line choke.

Schneider Electric Global