{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Does ‘automatic reactivate’ reset the overload?
Question:
As for the X80 DDO module, Reactivate has the options Programmed or Automatic If I select automatic will it reset the overload?


Answer:
No, ‘Automatic’ means if the outputs are cut off(physically), the rearmament is performed by the module each 10 second.