How to coordinate the start address of IOscanner at BMENOC0301 of M580 system to communicate with Quantum
Published date:
26 December 2018
Question:
How to coordinate the start address of IOscanner at BMENOC0301 of M580 system to communicate with Quantum?
Answer:
Inside IO scan configurator of M580 system, the RD Address/WR Address is referring to address of counterpart.
Since M580 starts from %MW0 while Quantum start from %MW1, you have to assign the address 99 at M580 IOscan configurator to correspond to the address 100 at Quantum.