Issue:
InFA or internal error 10 on the ATV630 and ATV930.
Product Line:
ATV630 and ATV930
Environment:
All
Cause:
The external supply voltage is to high.
The P24 voltage input for the customer 24vdc supply is monitored against
overvoltage. The error raise at P24 > 30.5vdc
Resolution:
Check the external 24V supply make sure its less than 30.5vdc
InFA or internal error 10 on the ATV630 and ATV930.
Product Line:
ATV630 and ATV930
Environment:
All
Cause:
The external supply voltage is to high.
The P24 voltage input for the customer 24vdc supply is monitored against
overvoltage. The error raise at P24 > 30.5vdc
Resolution:
Check the external 24V supply make sure its less than 30.5vdc
Released for: Schneider Electric Global