{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can I use a NetBotz NBPD0165 camera pod with older NetBotz appliances?
Issue:
Can I use a NetBotz NBPD0165 camera pod with older NetBotz appliances?

Product Line:
NetBotz

Environment:
NetBotz cameras

Cause:
NetBotz has released the NBPD0165 camera pod.

Resolution:

No, the camera pod NBPD0165 is not compatible with NetBots 3xx, 4xx, and 5xx devices. There are currently no plans to integrate the cameras into the older appliances. As of it's release, it is only compatible with the NetBotz 750 series appliances.

Schneider Electric Global

Explore more
Product:
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: