{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the optional control power transformer part number used in the enclosed ATS22 with the B10 mod?
Issue:
Transformer used in the enclosed ATS22 with the B10 Mod.

Product Line:
B10 Mod used in the Enclosed ATS22

Environment:
All

Cause:
Transformer part number.

Resolution:
When the B10 option is selected, transformer# 9070TF300D1 will be included in this enclosure.  If a transformer larger than this is needed, I would recommend contacting our drives quotes group. They provide support for custom enclosed drive and soft starter applications

Schneider Electric Global

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: