{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How does the Fast Stop work on the Altivar 320 drives?
Issue:
How does the Ramp Divider (DCF) affect the deceleration time when the Fast Stop function is used on the AT320 drives?

Product Line:
Altivar 320 ATV320 MACHINE drive

Resolution:
How to figure the resulting ramp time. When using the Fast stop assignment to a logic input (FST = LIx) or as the Type of Stop (STT = FST), the Ramp divider (DCF) affects the normal DEC setting:Fast stop ramp time = DEC divided by DCFDCF is adjustable from 0 to 10Examples:If DEC = 20sec and DCF = 2, then the fast stop ramp is 20 / 2 = 10secIf DEC = 20sec and DCF = 4, then the fast stop ramp is 20 / 4 = 5sec

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Global