{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
In IEC 60870-5-101/104 Master/Client Communication for BMXNOR0200 which data point is meant for General Interrogation command.
Issue:
In IEC 60870-5-101/104 Master/Client Communication for BMXNOR0200 which data point is meant for General Interrogation command.

Product Line:
BMXNOR0200H

Environment:
All

Resolution:
In IEC 60870-5-101/104 Master/Client Communication for BMXNOR0200 data point which is meant for General Interrogation command is C_IC.

Schneider Electric Global