{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Are spacers available for the leveling feet of NetShelter cabinets?
Issue:
It may be difficult to level a row of cabinets using the leveling feet only due to height differences in the concrete pad.

Product Line:
NetShelter SX, SV

Environment:
All versions and serial ranges.

Cause:
Cabinet rows need to be leveled.

Resolution:

Please use AR7605 spacer kit. Each kit includes 160 pieces: (120 x 8mm) and (40 x 2.25mm)

Schneider Electric Global