Issue:
What is FLU on the top left of HMI of ATV71?
Product Line:
ATV71
Environment:
All serial numbers
Cause:
Customer wanted to know what is the FLU code on the keypad.
Resolution:
FLU is a status of the drive meaning Motor fluxing in progress. Under 1.3 Settings in the Drive Menu, Motor Fluxing can be set to FnC (not cont), FCt (Continuous) or Fno (No or Function inactive).
• In [Continuous] (FCt) mode, the drive automatically builds up flux when it is powered up.
• In [Not cont.] (FnC) mode, fluxing occurs when the motor starts up.
CAUTION
Check that the motor will withstand this current without overheating.
Failure to follow this instruction can result in equipment damage.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.