Issue:
Programming analog input for 0-10V to control 30-60 Hz on an ATV212 Drive.
Product Line:
Altivar 212
Environment:
All
Cause:
Wants 0-10V to equal 30-60Hz
Resolution:
Yes, this is accomplished by adjusting the scaling of the applicable analog input so that the drive knows that 0%=30Hz.
If you're using VIA: Adjust F201 to 0%, F202 to 30Hz, F203 to 100% and F204 to 60 Hz.
If you're using VIB: Adjust F210 to 0%, F211 to 30Hz, F212 to 100% and F213 to 60 Hz.
For details on accessing these parameters please see the FAQ on ATV212 Basic Programming.
Programming analog input for 0-10V to control 30-60 Hz on an ATV212 Drive.
Product Line:
Altivar 212
Environment:
All
Cause:
Wants 0-10V to equal 30-60Hz
Resolution:
Yes, this is accomplished by adjusting the scaling of the applicable analog input so that the drive knows that 0%=30Hz.
If you're using VIA: Adjust F201 to 0%, F202 to 30Hz, F203 to 100% and F204 to 60 Hz.
If you're using VIB: Adjust F210 to 0%, F211 to 30Hz, F212 to 100% and F213 to 60 Hz.
For details on accessing these parameters please see the FAQ on ATV212 Basic Programming.
Released for:Schneider Electric Global