Issue:
Recommendation for SSC setting on ATS22 Softstarter.
Product Line:
Altistart 22, ATS22
Environment:
All serial numbers
Cause:
On a new installation, should it be On or Off?
Resolution:
Default is "On" which means that Acceleration (ACC) and Deceleration (DEC) are controlled by torque.
When SSC=On the soft starter will set automatically the Start-stop profile control voltage.
This configuration is suitable for most of the applications, and especially pumps.
Recommendation for SSC setting on ATS22 Softstarter.
Product Line:
Altistart 22, ATS22
Environment:
All serial numbers
Cause:
On a new installation, should it be On or Off?
Resolution:
Default is "On" which means that Acceleration (ACC) and Deceleration (DEC) are controlled by torque.
When SSC=On the soft starter will set automatically the Start-stop profile control voltage.
This configuration is suitable for most of the applications, and especially pumps.
Released for:Schneider Electric Global