{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is a competitive cross for Cutler Hammer 92-01943-01?
Issue:
Looking for a replacement HMI with a physical keyboard to replace a Cutler Hammer 92-01943-01.

Product Line:
Magelis HMIGK

Resolution:
The competitive cross for the Cutler Hammer 92-01943-01 is the HMIGK2310. The HMIGK is programmed with Vijeo Designer V6.2 SP5.1 or higher.

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.