{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
On ATV320, how to switch freq reference from CAN to AI1 by canopen if the drive is controlled by somachine blocks that do not allow to add bits onto CMD word?
If it is not possible to control CMD bits 11-15 by Somachine, the best way is to program ATV logic. Switching signal from PLC can be passed to the logic via FB parameter M001.
Logic will read M001 and depending on lowest bit it will switch reference from CAN to AI1.
See attached example for ATV320 configuration including ATV logic inside.

Schneider Electric Global

Attachment(s)
ATV320_logika_CAN-AI1 pro otacky.zip [76.44 KB]