{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What are the replacement interiors for the 9001BW Pendant control stations?
Issue:
Needs the replacement contacts or interior for 9001BW pendant stations

Product line:
Push Buttons and Operator Interface

Environment:
9001BW Pendant control

Resolution:
Note replace the * with the enclosure color Y = yellow, B = black R = red
9001BW92* - replacement interior is 9001BOC368
9001BW93* - replacement interior is 9001BOC368
9001BW94* - replacement interior is 9001BOC358
9001BW95* - replacement interior is 9001BOC359
9001BW96* - replacement interior is 9001BOC358
9001BW97* - replacement interior is 9001BOC359
9001BW98* - replacement interior is not available

9001BW90*U - replacement interior is 9001BOC366
9001BW91*U - replacement interior is 9001BOC359
9001BW94*U - replacement interior is 9001BOC358
9001BW100*U - replacement interior is 9001BOC367
9001BW102*U - replacement interior is 9001BOC367

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: