How is the value of motor torque (OTR) obtained in the ATV320 drive?
Published date:
05 March 2019
Issue:
How is the value of motor torque (OTR) obtained in the ATV320 drive?
Product Line:
ATV320
Environment:
All
Cause:
Wants to know how motor torque monitoring is achieved. Is it measured or estimated
Resolution:
On ATV320, this parameter will be estimated (the torque is estimated based on motor current measured).
The torque of motor is not measured by the drive. It is calculated from the measurement of motor
current.
OTR = (Iq / Iqn) * (PhirdRef / Phirn) in %
With: Iq : Current torque provide by the command to drive motor
PhirdRef : Flux provide by the command to drive motor
Iqn : Nominal Current torque compute with the motor name plate
Phirn : Nominal flux of the motor
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.