{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What does the suffixes W and WS mean on ATV320...W and ATV320...WS?
Issue :
Meaning of "W" suffix on the ATV320.

Product Line :
Altivar Drive

Environment :
ATV320

Cause :
Looking for an enclosed ATV320

Resolution :
The ATV320 that comes with the "W" or "WS" suffixes are both enclosed units. Enclosure rating is UL Type 12 /IP66.
"W" is without a Vario line disconnect switch
"WS" is with a Vario line disconnect switch

Schneider Electric Global