{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How do I create a Recipe with EcoStruxure Machine Expert?

Issue:
Usually the recipe is created on the HMI side with Vijeo Designer but there might be cases where the recipe needs to be be part of the controller application.


Product Line:
M241
M251

Environment:
SoMachine V4.1
EcoStruxure Machine Expert V1.0

Resolution:

1) From the Tool Tree, right-click on Application and add the Recipe Manager.

2) Add a Recipe Definiton.

3) Define the Recipe Column.  You can add the Variable and the Current Value.

4) Define the recipe by adding the ingredient.

5) Add a label name to each ingredient.

6) Create the new recipe and enter the value.

7) Create a new POU and use the LoadRecipe and WriteRecipe to test the recipe.  Those function blocks are part of the Recipe Management library which is automatically install when using the Recipe manager

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.