1.Issue
This FAQ describes how to animate a pre-defined image in Vijeo XD in V3.02.Enviroment
Vijeo XD V3.03.Resolution
For the current version of VXD software (VXD 3.0), it is not possible to directly animate the pre-defined image in Vijeo XD.Usually the work around is to add graphics above the pre-defined image. For example, as can be seen from the attached picture, we add a rectangular graphic above the tank to represent the level animation. The height of the graphic animation is linked to the variable--tank level.
Animation of pre-defined image will be added as a new feature in V3.2.
4. FAQ Applicable Conditions
FAQ also applies to VXD V3.1.Released for:Schneider Electric Global