Issue:
The user may require a specific parity setting on the Link150 (EGX150) when the transmission mode has been set to Modbus ASCII
Product Line:
Link150 (EGX150)
Resolution:
When the transmission mode is set to Modbus ASCII, the parity of the serial port is limited to EVEN. Unfortunately, parity cannot be adjusted to none or odd.
Released for:Schneider Electric Global