SBO upgrade process failed (SBO 1.8.x to SBO 1.9.x)
Published date:
10 April 2019
Upgrade failed when upgrading Automation Server from SBO version 1.8.x to 1.9.x
Log indicate:
(Device Administrator | View | Last Upgrade Log)
ERROR: Exception encountered during database upgrade : StartUpMode UpgradeDatabase : RecoverableException: d:\dev\rb-rb-1.9.2-system\source\server\nsp_servers\csc\LonTypes\source\Lon2MapFileUtil.cpp(185) Invalid Data Error: Invalid_Data (0x10000) in module Impex(57). "Map data is too old for type: public.lon2.devicetemplates.pid90003A8200E90401. You need to run the Lon Repair command in the latest version of workstation"
2019-04-10 07:14:02 INFORMATION: Database upgrade time: 5.28889 seconds
2019-04-10 07:14:02 INFORMATION: ============= End Configuration Database Upgrade =============
Source version: 1.8.1.79 Target Version: 1.9.2.45
Stteps
1. Upgrade Workstation and Automation Server to latest available version (SBO 1.8.1.3600)
2. Connect with Workstation to Automation Server
3. Select Server, right click Advanced | Repair LonWorks configuration ...
4. Select Next to repaire when indicated "Server needs to be repaired"
5. Finally upgrade to Version 1.9 using Device Administrator