{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to join together 2 Prisma P frameworks?
The Prisma P framework is delivered with the fixing elements necessary to join together two cubicles installed side by side.


It is recommended to choose the installation position of these elements based on the panels' configuration:
1. If horizontal busbars are installed at the top of the panel, then the 2 short screws have to be installed at the top and the 4 longer screws at the middle and bottom.
2. If horizontal busbars are installed at the bottom of the panel, then the 2 short screws have to be installed at the bottom and the 4 longer screws at the middle and top.
3. If horizontal busbars are not installed in the panel, then any of the 2 solutions above may be used.

The above instructions are meant to assure that the combination screws are not interfering with the installation of horizontal busbar supports or other mounting plates.