{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the maximum mounting depth of a 1070mm (42") deep NetShelter SX cabinet with no accessory mounting rails?
Issue:
A customer needs to know the maximum available mounting depth.

Product Line:
NetShelter SX 1070mm Deep

Environment:
All versions and serial ranges.

Cause:
A customer has very deep equipment and wants to know if it will fit into the cabinet.

Resolution:

The maximum spacing for an AR3100 is 35.75”. At this spacing, the rear accessory/PDU mounting rails must be removed.

Schneider Electric Global

Attachment(s)
NetShelter Max Depth for 1070mm Deep Cabinet with no Accessory Rails.jpg [28.75 KB]