In Ecostruxure Machine Expert, the function block MC_Movelocity_PTO has 4 JerkRatio inputs.

JerkRatio1-4 are used to change the shape of the S-curve.

JerkRatio1-4 are used to change the shape of the S-curve.
- JerkRatio1: Percentage of acceleration from standstill used to create the S-curve profile
- JerkRatio2: Percentage of acceleration to constant velocity used to create the S-curve profile
- JerkRatio3: Percentage of deceleration from constant velocity used to create the S-curve profile
- JerkRatio4: Percentage of deceleration to standstill used to create the S-curve profile
Released for: Schneider Electric Global