{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Video: How to configure the HMIBSC Edge Box as a 4G router
Question
How to configure the HMIBSC Edge Box as a 4G router


Description
1- Create the IP_Forwarding script
~# vi /etc/init.d/IP_Forwarding.sh
#!/bin/sh
loadkeys fr # To set the keyboard - optional if you prefer use a qwerty keyboard
echo 1 > /proc/sys/net/ipv4/ip_forward
iptables -t nat -A POSTROUTING -o usb0 -j MASQUERADE
Save file with :wq
2- Create a link in the correct run level
~# ln -s /etc/init.d/IP_Forwarding.sh /etc/rc3.d/S98IP_Forwarding #The RC number depend of your run level
3- Add the executable right for the script
~# chmod 755 /etc/init.d/IP_Forwarding.sh
~# ls -l /etc/init.d/IP_Forwarding.sh # rwxr-xr-x rights
4- ~# reboot


Keywords
Schneider Electric, HMIBSC, BSC, Edge Box, Configuration, 4G, router

Case author:
Lilian Cabos

Product Familly
IIOT Edge Box

Schneider Electric Global