{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can the new NetShelter SX 12U and 18U cabinets be stacked?
Issue:
A customer is asking if the new short NetShelter SX cabinets can be stacked.

Product Line:
NetShelter SX 12U and 18U

Environment:
All versions and serial ranges.

Cause:
A customer may want to stack these shorter cabinets.

Resolution:

These cabinets were not designed to be stacked, and should never be stacked. These are stand-alone cabinets, not stackable.

Schneider Electric Global