How to modify runtime security setting on EOTE V3.1 with USB drive
Published date:
03 December 2019
1. Issue
How to modify runtime security setting on EOTE V3.1 with USB drive
2. Environment
EOTE V3.1
3. Resolution
) Set In the [Project Explorer], select [Security] ➞ [Setting], and click [Export].
) Define the location and file name.
Note: To import the exported file to the panel, save the file to the root directory of USB memory with the specified folder and file name. Folder Name: UserManagement File Name: data.bin 3. ) Enter the encryption key. This key is used for importing and modifying user information. 4. ) To import user information from the panel, setting up scripts is required. 5. ) On the screen, touch the import switch. 6. ) Enter the encryption key. On the panel, the project user information is overwritten.
4. FAQ Applicable Conditions
FAQ also applies to Vijeo XD V3.0.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.