{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Power Monitoring Expert v8.x & 9.0 –EM6436 dual source meter consume S type license instead E type.
Issue
In PME v8.x and 9.0 when EM6436 dual source meter is added in MC, it consumes High-End device license instead of Entry Range device license.

Environment
PME Licensing

Cause
This appears to be a bug in PME v8.x and PME 9.0.

Resolution
Run attached hotfix (exe) file where PME is installed.

Note: In case of distributed architecture, run exe in Application Server.

Schneider Electric Global