Issue:
NEMA or IP rating has been requested.
Product Line:
SmartBunker FX
Environment:
All versions and serial ranges.
Cause:
There is no IP or NEMA rating listed in the Technical Specifications.
Resolution:
The SmartBunker FX is not IP/NEMA rated.
The current design of the enclosure does not provide an official dust or water rating. The only statement we can use is that there is an enhancement kit of the gaskets that can prevent vertical leakage from water sprinklers to enter the enclosure.
NEMA or IP rating has been requested.
Product Line:
SmartBunker FX
Environment:
All versions and serial ranges.
Cause:
There is no IP or NEMA rating listed in the Technical Specifications.
Resolution:
The SmartBunker FX is not IP/NEMA rated.
The current design of the enclosure does not provide an official dust or water rating. The only statement we can use is that there is an enhancement kit of the gaskets that can prevent vertical leakage from water sprinklers to enter the enclosure.
Released for:Schneider Electric Global