Issue :
Replacement connectors for ATV340 drive.
Product Line :
Altivar Drive
Environment :
ATV340, Altivar Machine, Altivar 340
Cause :
Lost connector kit
Resolution :
There are three different part numbers for the kit, depending on the drive frame size. A single connector piece is not available, order the complete kit only.

Drive Frame Size 1
Part# VW3A34001
ATV340U07N4 ATV340U15N4 ATV340U22N4 ATV340U30N4 ATV340U40N4
Drive Frame Size 2
Part# VW3A34002
ATV340U55N4 ATV340U75N4
Drive Frame Size 3
Part# VW3A34003
ATV340D11N4 ATV340D15N4 ATV340D18N4 ATV340D22N4
Replacement connectors for ATV340 drive.
Product Line :
Altivar Drive
Environment :
ATV340, Altivar Machine, Altivar 340
Cause :
Lost connector kit
Resolution :
There are three different part numbers for the kit, depending on the drive frame size. A single connector piece is not available, order the complete kit only.
Drive Frame Size 1
Part# VW3A34001
ATV340U07N4 ATV340U15N4 ATV340U22N4 ATV340U30N4 ATV340U40N4
Drive Frame Size 2
Part# VW3A34002
ATV340U55N4 ATV340U75N4
Drive Frame Size 3
Part# VW3A34003
ATV340D11N4 ATV340D15N4 ATV340D18N4 ATV340D22N4