Issue:
Wanting to control, the ATS22, with the Modbus network and also be able to use the remote keypad display.
Product Line:
Altistart 22
Environment:
All models and serial numbers
Cause:
N/A
Resolution:
The ATS22 soft starter has a built in display, as part of the soft starter. The RJ-45 port can be used for a remote mounted display keypad or for Modbus network. If the RJ-45 port is used for communications or for remote keypad the local display on the soft starter control board will still operate. The port can not be used for both a remote keypad and for Modbus communication.
Wanting to control, the ATS22, with the Modbus network and also be able to use the remote keypad display.
Product Line:
Altistart 22
Environment:
All models and serial numbers
Cause:
N/A
Resolution:
The ATS22 soft starter has a built in display, as part of the soft starter. The RJ-45 port can be used for a remote mounted display keypad or for Modbus network. If the RJ-45 port is used for communications or for remote keypad the local display on the soft starter control board will still operate. The port can not be used for both a remote keypad and for Modbus communication.
Released for:Schneider Electric Global