{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Do Vijeo Designer Events have an Active state?
Issue:
When setting the "Alarm & Event List" to Active for an Event Group, nothing is display during runtime when there are Events. The only settings that display Events are History and Log.

Product Line:
Vijeo Designer (all versions)

Resolution:
Events in Vijeo Designer have no concept of "state". In essence, an event is something that has occurred already in the past. Therefore is no such thing as an Active event in Vijeo Designer. When using the Alarm & Event summary, the setting "Alarm & Event List" can only be set to History or Log for Events. If monitoring states is required, it is recommended to use Alarms rather than Events.