Issue
After changing the calibration constants of the current probe in the ION meter using terminal access and command kctstp, the meter's phase angle for current does not change
Product
ION 7650
ION 7550
Environment
ION Setup
Front panel
Power Monitoring Expert
Cause
The phase angle correction is only applied to the kW, kVA, kVAR in the power meter module only
Resolution
Phase angle adjustments are used for power correction only.
After changing the calibration constants of the current probe in the ION meter using terminal access and command kctstp, the meter's phase angle for current does not change
Product
ION 7650
ION 7550
Environment
ION Setup
Front panel
Power Monitoring Expert
Cause
The phase angle correction is only applied to the kW, kVA, kVAR in the power meter module only
Resolution
Phase angle adjustments are used for power correction only.
Released for:Schneider Electric Global