{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
EcoStruxure Control Expert V14.0 can stop working by doing a right click on a LD or LL984 contact
1. Issue

EcoStruxure Control Expert V14.0 stops working by doing a copy, paste, or cut of a graphic element from another software (e.g. Vijeo Designer, Word), then using right click in a LD or LL984 editor on one of the following selections:
For LD: Link (vertical, horizontal), Derivation, Contact, Coil, Compare, Operate, Input and output pins of function blocks (CTU, ...)
For LL984: Link (vertical, horizontal), Contact, Coil, Values inside function blocks
2. Product Line

EcoStruxure Control Expert V14.0
3. Resolution

One possible workaround is to perform CTRL+C command in EcoStruxure Control Expert V14.0 software. By doing this we will avoid the shutdown of EcoStruxure Control Expert, if we do a right click on LD or LL984 editor.

The correction is brought in EcoStruxure Control Expert V14.0 with the installation of ControlExpert_V140_HF0544798R hot fix.

This unexpected behaviour is resolved in EcoStruxure Control Expert V14.1.

Schneider Electric Global