{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to perform a firmware upgrade on a M580 HSBY?
Issue
The M580 HSBY DDT structure has changed and customer needs to follow this procedure where are upgrading the firmware.

Product Line
Unity Pro, Control Expert, BMEH582040, BMEH584040, BMEH586040

Environment
Control Expert v14.0, BMEH584040 v2.90

Resolution
As soon as the firmware upgrade is done then:
  1. Connect to the CPU with Unity Pro/Control Expert (CPU must be in STOP or Run wait)
  2. Use the HSBY_BUILD_OFFLINE EF to pass the CPU in Standby with MOL
Image1