{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How is manage the M580 FDR server when a TsysT device is pulling by the PLC?
The TsysT devices are configured by the configuration tool "SoMove".
The M580 PLC are configured by the configuration tool "Ecostruxure Control expert".
When the configuration of the TsysT is realized, SoMove transfert the configuration to the TsysT. A Somove menu allows to transfert the configuration of the TsysT device inside the FDR server of the PLC. There are two options:
1) the transfer in the FDR server appears after each setting modification of the TsysT (a delay can be adjust after each modification).
2) The transfer in the FDR server can be active manually from SoMove.
Whatever the option, a message "command send with success" appears in SoMove. This message means that the configuration has been transmitted BY SoMove to the TsysT.
In fine, the transfer inside the FDR server of the PLC is performed by the TsysT if the set of configuration is compatible with the TsysT. (Firmware version must match). Otherwise the configuration is not performed.
It's recommended to verify the FDR functionality by replacing a TsysT (by seting a TsysT in a manufacturing default and to connect it to the PLC).