Issue:
How do I install the VW3A3600 on my ATV320?
Product Line:
Altivar 320 (compact version only)
VW3A3600 Option Card Module
Environment:
All models
Cause:
Installation Instructions
Resolution:
Installation instructions for the VW3A3600 Option Card Module (used only with the compact versions of the ATV320) can be found here, below, and are also attached.
“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Released for:Schneider Electric Global