{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can NTP sever of M580 be used externally as time provider?
  1. Issue

It is known that M580 could be used internally as the time provider for CRA when configured as NTP server.
Then can NTP server of M580 be used externally as time provider?

  1. Environment
N/A
  1. Resolution
Yes, as long as M580’s address is configured in the same network as NTP client and NTP client sets the M580’s address as NTP server, the M580 could be used externally as the time provider.

Schneider Electric Global