{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is it supported to add sound file for alarm in VXD/EOTE
  1. Issue
Is it supported to add sound file like mp3/wav for alarm in Vijeo XD / EcoStruxure Operator Terminal Expert .
  1. Environment
Vijeo XD / EcoStruxure Operator Terminal Expert V3.1.
  1. Resolution
No, user can’t add/import specified external sound file into EOTE for alarm, but can use the beep operation in project, the panel will start to beep when the trigger occurs.

Schneider Electric Global