Can we access Web server of Altivar Process ATV600, ATV900 variable speed drive via the RJ45 port on the Profinet card VW3A3627 inserted in the drive?
Profinet card VW3A3627 has its own webserver that is different from ATV process web server.
Using this profinet card you can access the web server of profinet card, but bear in mind that this card runs web server on java and today on windows 7 or windows 10 or any newer it is not supported.
Only if you use old PC with windows XP and enable java, then you will be able to access drive monitoring, diagnostic and network setting. See picture.
To access Altivar process web server, it is enough to either connect ethernet cable to Altivar embedded eth port or to add ethernet cable from second RJ45 port on profinet card and wire it to ATV embedded port. Then to use IP address of embedded ethernet communication for accessing ATV process web server.
Using this profinet card you can access the web server of profinet card, but bear in mind that this card runs web server on java and today on windows 7 or windows 10 or any newer it is not supported.
Only if you use old PC with windows XP and enable java, then you will be able to access drive monitoring, diagnostic and network setting. See picture.
To access Altivar process web server, it is enough to either connect ethernet cable to Altivar embedded eth port or to add ethernet cable from second RJ45 port on profinet card and wire it to ATV embedded port. Then to use IP address of embedded ethernet communication for accessing ATV process web server.
Released for: Schneider Electric Global